Compare versions of a project
Compare two different versions of a project by selecting two different committed changes in View history.
-
In the open project, select
View history.
-
In Version history, select
in two different commits to compare.
Tip: The differences between the commits are highlighted. -
(optional) To toggle the content that appears in Version history, select either:
- All. Toggle to show all content in the project.
- Updates. Toggle to show only the differences between the selected commits. This is the default.