Add a group
Groups determine the organization of a system. For example, a system may have filling and packaging groups.
-
In the main toolbar, select
Open dashboard page and then select Manage users and groups.
- On the dashboard page, under Groups, select Add.
- In Add Group, under Name, enter the name for the group.
- (optional) If users are created, under Assign user to groups, select the users to assign to the group.
- (optional) If roles are created, under Assign roles to group, select the roles to assign to the group.
-
Select Add.
Tip: To create a group in Project view, under Security, right-click Groups to add a group, or select a group to add a subgroup, and then select .