Add a role
Roles determine the responsibilities of users in a system. For example, a system may have engineering and supervisory roles.
-
In the main toolbar, select
Open dashboard page and then select Manage users and groups.
- On the dashboard page, under Roles, select Add.
- In Add Role, under Name, enter the name for the role.
- (optional) If users are created, under Assign users to role, select the users to assign to the role.
- (optional) If groups are created, under Assign groups to role, select the groups to assign to the role.
-
Select Add.
Tip: To create a roles in Project view, under Security, right-click Roles and then select .