Apply a stylesheet to a report
Use the StyleSheet property to specify an instance of the selected style to apply to the report.
The units of measurement in reports are specified in FactoryTalk Optix Studio options. See Set options. The language that you select for a project determines the default unit of measurement. For example, if you set the language option to en-US, FactoryTalk Optix Studio uses inches as the default unit of measurement for reports.
- In Project view, select your Report# object.
- In Properties, in StyleSheet, select the drop-down arrow to select the stylesheet.