Push Agent
The Push Agent script sends data from a data logger to the cloud.
Operation
Push Agent periodically acquires data from a data logger and sends the data to the cloud in the JSON format. Push Agent implements the store and forward mechanism that acquires data from a data logger and saves the data in an auxiliary store from which the data is extracted and sent to the cloud.
Transfer modes
Push Agent supports the following transfer modes:
- By line. Sends one line of the data logger per packet.
- By variable. Sends one or more variables with their related information.
Tip: If the data logger mode is set to Value change, the sampled values change only if one of the monitored variables changes. Push Agent sends the values of a certain variable only if the variable value differs from the previously sent value.