Configure a video
Insert a video file container to your project, and place a video file in it. Use video files local to the project or remote videos.
- In Project view, in UI, right-click a container and then select .
-
In Path, either:
- Select Browse and select the local video to display.
Tip:
To find items, start typing the item name to find in Select file.
If the file does not appear in Select file, select
Import file(s) and in Import file(s), select the file to import and then choose Select. - Enter the address of the remote video file to display.
- Select Browse and select the local video to display.
-
(optional) Set the auto play options.
- Auto play. Video will be played automatically. Disabled by default.
- Muted. Video will play without sound. Disabled by default.
- Loops. Specifies the number of times video will play. The default is 1.
- (optional) Muted.
- (optional) Set the Appearance and Size and layout properties.