Navigate a trend chart
Navigate the X-axis and Y-axis of a trend chart in the Normal trend mode.
-
Select a point and drag it horizontally to navigate the X-axis.
Tip: If the Follow property is set to True, automatic scrolling stops when you interact with the graph. To restart the automatic scrolling of the X-axis, scroll the X-axis to the current instance.
- Select a point and drag it vertically to navigate the Y-axis.
- Select a pointer and drag it diagonally to browse on both axes.