Draw a rectangle or square
Use the Rectangle tool to draw rectangles or squares.
- In Project view, double-click the container to include the object.
-
In the editor toolbar, select
Rectangle.
- In the editor, position the crosshair where the square or rectangle is to begin.
- Drag to draw a rectangle or square.