Add a screen instance
Create an instance of a screen type and modify the screen instance properties.
Prerequisites
-
Right-click a node to contain the screen object and select .
The screen object instance appears under the node and inherits the properties of the screen type.
-
(optional) In Properties, set the screen instance properties.
For more information, hover-over the properties.
- (optional) Add objects to the screen instance.