Delete a method from an event
Delete an event to remove the event and the event methods from the project. You cannot delete the default events for a pre-configured element.
- In Project view, select an object.
- In Properties under Events, expand the user-defined event.
- Select the event and then press Delete.