Configure a change event
Trigger methods if the value of a variable or object property changes.
Tip: If you use a controller tag in a change event, the tag always updates at runtime, even if the FactoryTalk Optix Application does not display the tag value.
- In Project view, select an object or a variable.
-
In Properties, right-click a variable or a property and select .
Tip: If needed, select
to add a variable. -
In Events, next to VariableChanged, select
.
-
Select a method:
- For global methods, expand Commands.
- For local methods, expand the nodes that expose methods (for example, a DataGrid node exposes a Refresh method), or expand the node related to a specific NetLogic.
- (optional) If the method requires arguments, expand the method and set arguments.
- (optional) Select more methods by repeating 3 through 5.