Configure a range transitioned event
Trigger methods if the value of a variable or object property is in or out of a specific range.
- In Project view, select an object or a variable.
-
In Properties, right-click a variable or a property and select .
Tip: If needed, select
to add a variable. -
In Events, from Transition select:
-
In (Exclusive)
-
Out (Exclusive)
-
In (Inclusive)
-
Out (Inclusive)
Item Description 
Range 
Value transition 
Method execution -
-
Set the From property.
Tip: You can enter the threshold value or add a dynamic link to the threshold value. For more information about dynamic links, see Create dynamic links.
-
Set the To property.
Tip: You can enter the threshold value or add a dynamic link to the threshold value. For more information about dynamic links, see Create dynamic links.
-
Next to VariableTransitioned, select
.
-
Select a method:
- For global methods, expand Commands.
- For local methods, expand the nodes that expose methods (for example, a DataGrid node exposes a Refresh method), or expand the node related to a specific NetLogic.
- (optional) If the method requires arguments, expand the method and set arguments.
- (optional) Select additional methods.