Associate the LED status with the switch
Turn the LED object on and off with the switch.
- In Project view, select LED1.
-
In Properties, create a dynamic link between Active and .
For more information about dynamic links, see Create dynamic links.