InformationModel.MakeAnalogItem(browseName, dataTypeId)
Create a project analog variable derived from AnalogItemType, which contains the data type indicated and returns a corresponding IUAVariable C# object.
static IUAVariable MakeAnalogItem(QualifiedName browseName, NodeId dataTypeId);
Arguments
browseName(QualifiedName)- The
BrowseNameof the new variable. -
dataTypeId(NodeId) -
The Data type contained in the new variable.
Tip: A node inside theDataTypesclass represents the Data type. For example,OpcUa.DataTypes.Boolean.
Returns
IUAVariable- A C# object that corresponds to the project variable created.
Example
The following example shows an API that creates an analog variable (MyAnalogVar) that contains a float data type:
var myVar = InformationModel.MakeAnalogItem("MyAnalogVar", OpcUa.DataTypes.Float);
Owner.Add(myVar);