RemoteVariableSynchronizer.Remove(variables)
Depending on the overload, removes a variable or a list of variables from the RemoteVariableSynchronizer object on which it is invoked.
void public void Remove(IUAVariable variables);
void public void Remove(RemoteVariable variables);
void public void Remove(IEnumerable<IUAVariable> variables);
void public void Remove(IEnumerable<RemoteVariable> variables);
Argument
variables(IUAVariable)- The
IUAVariableC# object to add to the object on which the method is invoked. variables(RemoteVariable)- The
RemoteVariableC# object that identifies a cell of a one-dimensional or multidimensional array to be added to the object on which the method is invoked. variables(IEnumerable<IUAVariable>)- The
IUAVariablelist to be added to the object on which the method is invoked. -
variables(IEnumerable<RemoteVariable>) - The
RemoteVariablelist to be added to the object on which the method is invoked.
Examples
In the following example, a variable
speed is removed from the variableSynchronizer object.
variableSynchronizer.Remove(speed);
In the following example, the
10 index variable is removed from the variableSynchronizer object within the arrayVariable array.
variableSynchronizer.Remove(new RemoteVariable(arrayVariable, 10));
In the following example, the
10.5 index variable is removed from the variableSynchronizer object within the scalarVariable multidimensional array.
variableSynchronizer.Remove(new RemoteVariable(scalarVariable, new uint[] { 10,5 }));