IUANode.GetVariable(browsePath)
Returns an IUAVariable C# object. The returned object corresponds to the first child variable of the node on which the method is invoked. The returned object name corresponds to the argument.
IUAVariable GetVariable(string browsePath);
Arguments
browsePath(string)-
Can be either:
- The
BrowseNameof the object - The path of the object in the information model, uniquely expressed as a sequence of
BrowseNamevalues separated by/
- The
Returns
IUAVariable- A C# Object that matches the requested variable.
Examples
The following examples show a returned C# object that corresponds to the
Speed variable of the Motor1 object:
var currentSpeed = Project.Current.GetObject("Motor1").GetVariable("Speed")
var currentSpeed = Project.Current.GetVariable("Motor1/Speed");