IUANode.Get(browsePath)
Returns an IUANode C# object that corresponds to the first child node of the node on which the method is invoked. The returned object name corresponds to the argument.
IUANode Get(string browsePath);
Arguments
browsePath(string)-
Can be either:
- The
BrowseNameof the object - The path of the object in the information model, uniquely expressed as a sequence of
BrowseNamevalues separated by/
- The
Returns
IUANode- A C# object that matches the requested node.
Examples
The following examples show a returned C# object that corresponds to the
Motor1 node that is a child of Machine1:
var motor1 = Owner.Get("Machine1").Get("Motor1");
var motor1 = Owner.Get("Machine1/Motor1");