IUAVariable.RemoteWrite(value, timeoutMilliseconds)
Writes the value passed in the first argument in the variable on which it invokes. The second optional argument sets the timeout period.
void RemoteWrite(UAValue value, double timeoutMilliseconds);
Arguments
value(UAValue)- The value to write.
-
timeoutMilliseconds(double) -
The timeout period, expressed in milliseconds, after which the API throws an exception.Tip: If not specified, the default value of the argument is
30000(30 seconds).
Example
In the following example, the
42 value is written in the Speed variable.
var currentSpeed = Project.Current.GetVariable("Model/Motor/Speed");
currentSpeed.RemoteWrite(42);