IUAVariable.RemoteRead(timeoutMilliseconds)
Returns the value of the variable on which it invokes. The optional argument sets the timeout period.
UAValue RemoteRead(double timeoutMilliseconds);
Arguments
-
timeoutMilliseconds(double) -
The timeout period, expressed in milliseconds, after which the API throws an exception.Tip: If not specified, the default value of the argument is
30000(30 seconds).
Returns
UAValue- The value of the variable.
Example
In the following example, the
Speed variable value is read and given in an information message.
var currentSpeed = Project.Current.GetVariable("Model/Motor/Speed");
var value = currentSpeed.RemoteRead();
Log.Info(value.ToString());