LogicObject.SetAlias(string, IUANode)
Sets the value of an alias, or the node the alias points to.
void SetAlias(string aliasName, IUANode pointedNode);
Arguments
-
aliasName(string) - The
BrowseNameof the alias to set. pointedNode(IUANode)- A
Nodeto which the alias must point to.
Example
The following example shows the MotorInstance alias that points to the Motor1 node.
var myMotorInstance = Project.Current.FindObject("Motor1");
LogicObject.SetAlias("MotorInstance"), myMotorInstance);