InformationModel.MakeAlias(browseName)
Creates an alias and returns a corresponding IUAVariable C# object.
static IUAVariable MakeAlias(QualifiedName browseName);
Arguments
browseName(QualifiedName)- The
BrowseNameof the new alias.
Returns
IUAVariable- A C# object that corresponds to the project object created.
Example
The following example shows an alias that is created in the Motor1 object of the FactoryTalk Optix Studio project:
var modelFolder = Project.Current.Get("Model");
var alias = InformationModel.MakeAlias("CurrentMotor");
modelFolder.Add(alias);
modelFolder.SetAlias("Model", Project.Current.Find("Motor1"));