Delete an event logger
Delete an event logger by removing the event logger object in Project view.
Tip: You can disable an event logger without the need to completely remove the logger from the project. For more information, see Edit an event logger.
In Project view, right-click an event logger object and select Delete.