Configure a recipes editor
Configure the recipes editor to manage recipes at runtime.
-
From the toolbar, select
Template Libraries.
- In Libraries, search for Recipes Editor.
- Under Components, drag Recipes Editor onto Page4 (type) in Project view.
- Select Close.
- In Project view, select RecipesEditor1.
-
In Properties, set Horizontal alignment to Stretch.
The object adjusts its width to the container at runtime.
- In Project view, select RecipesEditor1.
-
In Properties, create a dynamic link between RecipeSchema and .
For more information about dynamic links, see Create dynamic links.
- Right-click RecipesEditor1 and select Execute Setup.