Configure a navigation panel
Configure a navigation panel to switch between different panels at runtime.
-
In Project view, double-click MainWindow (type).
The window type opens in the editor.
-
Right-click MainWindow (type) and select .
Navigation panel appears in the main window and is not positioned.
-
In Properties, set Horizontal alignment and Vertical alignment to Stretch.
The navigation panel occupies the entire height and width of the main window and covers the logo.
-
Set Top margin to 55.
The navigation panel no longer covers the logo.
- Drag Page1 (type), Page2 (type), Page3 (type), and Page4 (type) onto NavigationPanel1.