Variables
A variable is an element that represents a figure or a characteristic of an object and specifies the value of that characteristic.
Variable overview
Each variable:
-
Contains a DataType attribute
-
Can be structured to contain other variables
-
Contains descriptive attributes
-
Cannot contain objects
Tip: You cannot remove properties from predefined objects. For example, you cannot remove the Text property from a Label object.
Variable examples
For example, a variable can represent:
- The speed of a physical object
-
The Speed variable with a numeric (Int32) value defines the speed of the Motor object.
- A style characteristic of a graphic object
-
The Text color variable defines the color of the Label object
- Various object properties
-
A dynamic link to the EmbeddedDatabase1 object defines the Store variable value.