An object is an element that identifies a physical object such as a motor or a non-physical object such as a digital alarm.
Object components
An object can contain:
Display name
Description
Variables
Nested objects
Object example
A physical motor is a mechanical object with specific operational characteristics such as acceleration, speed, and torque. The Motor object in the project is an object that contains the same properties.
Figure 1. Motor object properties