InformationModel.SetTranslation(localizedText)
Updates a translation associated with an existing key, based on the argument properties.
void SetTranslation(LocalizedText localizedText);
Arguments
localizedText(LocalizedText)- A C# object with the
TextId,Text, andLocaleIdproperties that identify the key and related translation to be updated.
Example
The following example shows an API that writes the New translation string for the en-US locale associated with the Key1 key.
var localizedText = new LocalizedText("Key1", "New translation", "en-US");
InformationModel.SetTranslation(localizedText);