Example: Protocol configuration in event mode
An example of a NetLogic contained in the serial Port object that uses the event mode to read data sent asynchronously from a device. The OnClick method, linked to the button pressing event, enables you to stop the current reading and start a new reading.
To use the event mode, you must set the Timeout property to 0. This way, ReadBytes will be blocking as long as the requested data do not arrive on the serial port.
You can stop the reading with the CancelRead method, or the Close method. In both cases, a ReadCanceledException exception is generated. To carry out a clean close of the NetLogic, you must terminate any pending read operations by calling the Close method in the NetLogic Stop.
You can download a sample project from ../../../downloads/SerialPortDemoEventMode.zip.
public class RuntimeNetlogic1 : BaseNetLogic
{
private SerialPort serialPort;
private LongRunningTask task;
public override void Start()
{
serialPort = (SerialPort)Owner;
serialPort.Timeout = TimeSpan.FromMilliseconds(0.0);
task = new LongRunningTask(Run, Owner);
task.Start();
}
[ExportMethod]
public void OnClick()
{
// Cancel current read
serialPort.CancelRead();
task.Cancel();
// Start new read
task = new LongRunningTask(Run, Owner);
task.Start();
}
private void Run()
{
while(!task.IsCancellationRequested)
{
try
{
// Block until 3 bytes arrive on serial
var result = serialPort.ReadBytes(3);
foreach (var b in result)
Log.Info(String.Format("0x{0:x2}", b));
}
catch (ReadCanceledException ex)
{
// In case of read canceled, exit from the loop
Log.Info(ex.Message);
return;
}
catch (Exception e)
{
Log.Error(e.Message);
}
}
}
public override void Stop()
{
// Explicit call to Close to cancel pending read (if any)
serialPort.Close();
task.Cancel();
}
}