IUANode.FindObject(browseName)
Returns an IUAObject C# object. The returned object corresponds to the first child object found in the node children on which the method is invoked. The returned object name corresponds to the argument.
IUAObject FindObject(string browseName);
Arguments
browseName(string)- The
BrowseNameof the node to find.
Returns
IUANode- A C# object that corresponds to the object found.
Example
The following example shows a returned C# object that corresponds to the first
Motor object child of the project root node:
var motor = Project.Current.FindObject("Motor");
var currentSpeed = motor.GetVariable("Speed").Value;