IUANode.Remove(child)
Removes a project node that corresponds to the C# object passed in the argument.
void Remove(IUANode child);
Arguments
child(IUANode)- A C# object that corresponds to the project node to add.
Example
The following example shows that the
MyLabel label child of the Panel1 object is removed from the project:
var myPanel = Project.Current.FindObject("Panel1");
var objToRemove = Project.Current.FindObject("MyLabel");
myPanel.Remove(objToRemove);