Log.Node(node, verbose)
Returns a string that contains the path of the node passed in the argument. The second argument is optional and inserts the NodeID and object type in the returned string.
static string Node(IUANode node, bool verbose);
Arguments
-
node(IUANode) - The node for which the path is to be generated in a string format.
-
verbose(bool) -
false(default)- Does not insert additional information in the string returned.
true- Inserts the
NodeIDand object type in the string returned.
Returns
string- The path of the node passed as the argument. Based on the
verboseargument value, it can also contain theNodeIdand the object type.
Examples
The following example shows an API that generates a message consisting of the Error on node
string and the NetLogic path, returned as a string by the Log.Node API:
Log.Info("Error on node " + Log.Node(LogicObject);