Create the System object
The System object allows users to view and configure certain system variables, such as the date and time, device, display, and application settings for the FTOptixApplication.
Create one System object per project.
- In Project view, right-click Model and then select . System1 appears in Project view.