Move an object
Move an object in the editor to position objects as they will appear at runtime. All of the objects in a container move with the container.
To move an object
- In the editor, select and drag the object.
-
In Project view, select the object and then in Properties change:
- Horizontal alignment. Enter the value for the space between the object and the X-axis.
- Vertical alignment. Enter the value for the space between the object and the Y-axis.
Tip: The position of the object in Project view determines the order of objects on the Z-axis compared to other objects in the same container. Objects lower in the tree appear higher in the order on the Z-axis.