Configure the editor grid
Configure the grid in the editor to show or hide the grid, align objects in the grid, and size the grid.
-
In Project view, double-click a container object, or select
.
The editor opens in a new tab. -
In the editor toolbar, select
Grid settings.
-
Select the option to configure the grid:
- Grid Visible. Toggle showing the grid in the editor.
- Snap to grid. Align the edges of objects with the grid.
- Grid size. Specify the size of the grid in pixels.