FTP Server configuration
You can enable a File Transfer Protocol (FTP) server in your FactoryTalk Optix Application.
The runtime script
FTPServerLogic enables an FTP server within a FactoryTalk Optix Application. The script is found in the Scripts category in Template Libraries.
Important: You should start and stop the server only by using the exported OPC UA methods:
StartFtpServer and StopFtpServer.Required packages
You must install stable versions of the following required NuGet packages:
See NuGet packages.
Required parameters
The FTP server requires the following parameters to be configured:
| Parameter | Description | Configuration |
|---|---|---|
IPAddress |
IP address assigned to the server. | The default value is set to 127.0.0.1. |
Port |
Port assigned to the FTP server, | The default value is 21. |
FilesystemRoot |
FTP server exposes only a fraction of the local filesystem to client | On OptixPanel, you can only set either:
|
MinimumPASVPort |
Minimum port number for managing file listing and file transfer. | This value must be greater than the default 1024. |
MaximumPASVPort |
Maximum port number for managing file listing or file transfer. | This value must be greater than MinimumPASVPort. The default value for MaximumPASVPort is 1100. |
Username/Password |
FTP Server login credentials | |
ServerCertificateFile |
Server public certificate file, according to standard X509v3 and with .der extension. | It must be found in the FTOptixApplication/ProjectFiles/PKI/Own/Certs directory. If specified, the private key must also be specified. If not specified, it is automatically generated at runtime in the FTOptixApplication/ApplicationFiles/PKI/Own/Certs directory. |
ServerPrivateKeyFile |
Server private key file, with ASCII Base64 encoding and .pem extension. | It must be found in the FTOptixApplication/ProjectFiles/PKI/Own/Certs directory. If specified, the certificate must also be specified. If not specified, it is automatically generated at runtime in the FTOptixApplication/ApplicationFiles/PKI/Own/Certs directory. |
UseFtps |
Determine protocol to use, FTP or FTPS. | The FTP server is started/stopped via the StartFtpServer/StopFtpServer methods. |