Enable PowerFlex tags in a project
-
In Project view, select DriveConnectionDesignTimeNetLogic and in Properties, set up the following PowerFlex parameters:
- Update rate
- IPAddress
- PFType
-
To create a PowerFlex model, right-click on DriveConnectionDesignTimeNetLogic and execute the GetPowerFlexModel method.
The model is available in a new directory named with the PowerFlex type, its IP address, and update rate. For examplePF755TM_10.76.38.210_10sec.
-
To add another PowerFlex drive, repeat steps 1 and 2.