OPC UA and ODBC database data types
Table 1. Data types map
| FactoryTalk Optix data type |
Microsoft® SQL Server data type |
MySQL data type |
Data type returned by a queried SQL database |
| Boolean |
BIT |
BIT(1) |
Boolean |
| Integer |
BIGINT |
BIGINT |
Int64 |
| UInteger |
BIGINT |
BIGINT |
Int64 |
| byte |
SMALLINT |
SMALLINT UNSIGNED |
Int16 |
| SByte |
SMALLINT |
TINYINT |
Int16 |
| Int16 |
SMALLINT |
SMALLINT |
Int16 |
| UInt16 |
INT |
MEDIUMINT UNSIGNED |
Int32 |
| Int32 |
INT |
INT |
Int32 |
| UInt32 |
BIGINT |
BIGINT UNSIGNED |
Int64 |
| Int64 |
BIGINT |
BIGINT |
Int64 |
| UInt64 |
BIGINT |
BIGINT UNSIGNED |
Int64 |
| Float |
REAL |
FLOAT |
Double |
| Double |
FLOAT |
DOUBLE |
Double |
| DateTime |
DATETIME |
DATETIME(3) |
DateTime |
| String |
TEXT |
TEXT |
String |
| NodeId |
VARBINARY (max) |
BLOB |
NodeId |