Built-in aliases
The built-in aliases include Window, RecipeSchema, and Session aliases.
Window aliases
You can use the alias to reference to the application window properties and graphical objects that are present in that window.
RecipeSchema aliases
At design time, the project root node contains an alias for each RecipeSchema instance in the project. This alias has the same name as the related RecipeSchema object. The project also contains a Panel loaders object. Access the RecipeSchema aliases from any node that have the same BrowseName as the corresponding objects in the project. For example, a PanelLoader1 alias is generated for a PanelLoader1 object.
Tip: Aliases for Recipe Schema objects are created inside the project root node.
Session aliases
The alias points to the Session node that exists only at runtime. This alias contains several nodes that have values based on the user and session locale. At design time. this alias is always available for graphic objects and types.