Configure the speed panel (type)
Add a label, gauge, and a button that changes panels.
- 
        Create a speed label:
        
- In Project view pane, right-click SpeedPanel (type) and select .
 - 
            Hover-over the label, select 
, and enter SpeedLabel.
           - In Properties pane, set Text to Speed.
 
 - 
        Create a speed circular gauge:
        
 - 
        Create a button that changes panels:
        
- In Project view, right-click SpeedPanel (type) and select .
 - 
            Hover-over the label, select 
, and enter ChangePanelButton.
           - In Properties, set the Text property value to Change Panel.
 - 
            In Events, next to MouseClick event, select 
 and select .
           - Under Input arguments, create a dynamic link between NewPanel and