Configure the main panel (type)
Add and configure a panel loader that defaults to the speed panel.
- In Project view, right-click MainPanel (type) and select
-
Hover-over the panel loader, select
, and enter MainPanelLoader.
-
In Properties pane, create a dynamic link between Panel and .
For more information about dynamic links, see Create dynamic links.