Develop a contact form
Develop a contact form that sends emails to a predefined address.
Prerequisites
To develop the project
- Develop a NetLogic for sending emails.
- Create the contact form interface.
- Save the project.
Select Run to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.