Develop an archives manager
Use the preconfigured Zip Unzip NetLogic to create, extract, and password-protect ZIP archives.
Prerequisites
To develop the project
- Add the Zip Unzip NetLogic.
- Create the interface elements.
- Save the project.
Select Run to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.