Develop buttons for closing and shutting down
Create buttons that close the FactoryTalk Optix Application and shut down the host system.
Important: Pressing Shut down system immediately shuts down the host operating system on which the FactoryTalk Optix Application runs.
Prerequisites
To develop the project
- Create a button that closes the application.
- Develop a NetLogic that shuts down the host system.
- Create a button that shuts down the host system.
- Arrange the interface elements.
- Save the project.
Select Run to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.