Create a NetLogic that fetches UI
Create a NetLogic that fetches UI elements from the OPC UA server.
Set the default external code editor. See Set the default code editor.
To create a NetLogic that fetches UI
- In Project view, right-click MainWindow (type) and select .
-
Hover-over the NetLogic, select
, and enter UIFetcher.
-
Double-click the NetLogic.
The external code editor opens.
-
In the code editor, replace the existing code with the following code:
#region StandardUsing using System; using FTOptix.Core; using FTOptix.CoreBase; using FTOptix.HMIProject; using UAManagedCore; using OpcUa = UAManagedCore.OpcUa; using FTOptix.NetLogic; using FTOptix.UI; using FTOptix.OPCUAServer; #endregion public class UIFetcher : FTOptix.NetLogic.BaseNetLogic { public override void Start() { myDelayedTask = new DelayedTask(LoadRemotePanel, 2000, LogicObject); myDelayedTask.Start(); } public void LoadRemotePanel() { var clientPanelLoader = (PanelLoader)LogicObject.Owner.Get("ClientPanelLoader"); var remoteMainPanel = Project.Current.Get("UI/RemotePanels/MainPanel"); if (remoteMainPanel == null) { Log.Error("Remote server main panel not found"); return; } clientPanelLoader.ChangePanel(remoteMainPanel.NodeId, NodeId.Empty); } [ExportMethod] public void ReloadRemote() { Start(); } public override void Stop() { // Insert code to be executed when the user-defined logic is stopped myDelayedTask.Dispose(); } private DelayedTask myDelayedTask; } - Save the code.