Set the default code editor
We recommend using Microsoft Visual Studio 2022 or Microsoft Visual Studio Code as the default code editor.
Tip: Some development assistance features may not be available when using a different code editor.
Prerequisites
Download and install the preferred code editor.
To set the default code editor
-
In FactoryTalk Optix Studio, select
FactoryTalk Optix Studio Options.
-
In the dialog, from the Preferred code editor drop-down menu, select an option.
Tip: The Automatic option sets Visual Studio as the default editor. If Visual Studio is not available, Visual Studio Code is used as the default editor instead.
- Restart FactoryTalk Optix Studio.