Create an analog variable
Create an analog variable that indicates temperature.
- In Project view, right-click Model and select
-
Configure the variable:
- In Properties, set the AnalogVariable1 (Float) property value to 50.
- Next to the property value, select <None> and select Temperature: degree Fahrenheit
- Under EURange, set Low limit to -10.
- Set the High limit to 60.
- Set the Constrain to True.