Create a linear gauge
Create a linear gauge that shows the temperature.
- In Properties, right-click MainWindow (type) and select .
- In Properties, set the Editable variable value to False.
-
Create a variable:
For more information about dynamic links, see Create dynamic links.
-
Link the variable alias:
- In Properties, create a dynamic link between Value and .
- Create a dynamic link between Minimum value and .
- Create a dynamic link between Maximum value and .
For more information about dynamic links, see Create dynamic links.