Project encryption on a client device
Encrypt projects on any device with FactoryTalk Optix Update Server installed.
Encryption scope
Project YAML files, which represent the project information model, are transferred as encrypted binary files on client devices. For more information, see Project source format.
By default, Emulator components are encrypted. You cannot disable the encryption of Emulator components.
Encryption operation
Client devices generate public encryption keys based on the current hardware and Windows keys. The public encryption keys in EncryptionKey.bin are stored on the client devices in the Runtime folder. The encrypted application is tied to the specific client device hardware.
Encrypted projects cannot be copied to or run on different client device. Exporting an encrypted project to a USB device or folder does not encrypt the compiled project.
Tip: You can upload encrypted projects from device while opening a project even if you are logged into a different organization than the organization used to develop the project. For more information, see Open a project.