Manage client devices
Add, remove, duplicate, and select target client devices available in the network.
The default target client device, the Emulator, runs locally on the development computer. The Emulator is useful for testing FactoryTalk Optix Applications and does not require you to install the FactoryTalk Optix Application Update Service software.
Tip: The Emulator runtime stops automatically after two hours even if a valid license is present on the device. If you need to test your application for a longer period of time, export the application. See Export a FactoryTalk Optix Application.
Tip: Rebooting the Emulator is not supported so that you do not accidentally reboot a device on which Windows® is installed.