Import a FactoryTalk Optix Application
To deploy an exported FactoryTalk Optix Application, move the file to the client device and run the file.
Prerequisites
To import a FactoryTalk Optix Application
-
Move the exported files to the client device.
For example, attach the USB drive with the exported application to the client device.
-
Run FactoryTalk Optix Application on the client system:
-
On Windows® client devices, double-click FTOptixRuntime.exe.
-
On Linux client devices, in the terminal, navigate to the FTOptixRuntime file folder and enter ./FTOptixRuntime.
-
On OptixPanel, access the web interface and then select Import under Load application from USB.
-